Promass F sensor type flowmeter solving dual phasing issue
Porosity of Tomato pulp causing dual phasing
One of our customer manufacturing Tomato pulp faced problem of improper batch counting of the flow meter. Flow rate comes as low as 700 kg/hr sometimes which is low for flow meter of 2 inch line size.
Promass F sensor type flowmeter Solving Dual Phasing
Promass F sensor type flowmeter Solving Dual Phasing issue at the time of tomato pulp batching
Porosity of the Tomato Pulp causing dual phasing
Flow rate comes as low as 700 kg/hr sometimes which is low for flowmeter of 2 inch line size. Porosity of the Tomato Pulp causing dual phasing. The accuracy of the flowmeter varied a lot due to the above reasons causing improper batch counting of the flowmeter.
Promass bent tube F sensor solving issue of dual phasing
After installation of the F sensor the flowmeter started giving accuracy in the reading we within the customer limts. Customer had advantages to be able to use the flowmeter for packaging of the Tomato pulp in the Aseptic packages with the both national and international standard of accuracy of packaging.